Salesforce

Cool Cursor Contest!

« Go Back

Information

 
TitleCool Cursor Contest!
URL NameCool-Cursor-Contest
Summary
Details
Recently, two of our Simcenter Testing application engineers squared off in a contest - to create the coolest example of using cursors in Simcenter Testlab possible.

The results are below!  The following rules were used when creating these examples:
  • Displays and cursors had to be created from scratch - no premade examples.  This way, every step used to make the examples can be seen.
  • Examples could be created in Simcenter Testlab or Simcenter Testlab Neo.  Since displays and cursors are the same in both applications, the examples can be done in either platform. 
The examples created included:
1. Automatic Peak Cursor
2. Frequency, Spectrum, Order Processing Cursor
3. Matrix-Heatmap Display and Cursors
4. Overlay Data from Two Spectral Maps using Coupled Cursor
5. Order Cursor and Point Cloud Display
6. Non-linear Order Cursor


Enjoy!
 
Example 1: Automatic Peak Cursor
Direct YouTube link: https://youtu.be/9Bu-ElSdcCc
Highlights (with Detailed Link):
 
Example 2: Frequency, Spectrum, Order Processing Cursor
Direct YouTube link: https://youtu.be/_3dbcoiSKBw
Highlights (with Detailed Link):
 
Example 3: Matrix-Heatmap and Cursors
Direct YouTube link: https://youtu.be/UsOC0Y5eUKQ
Highlights (with Detailed Link):
 
Example 4: Overlay Data from Two Spectral Maps using Coupled Cursor
Direct YouTube link: https://youtu.be/YNmNoJvYy5o
Highlights (with Detailed Link):
 
Example 5: Order Cursor and Point Cloud Display
Direct YouTube link: https://youtu.be/J6NXDDCshys
Highlights (with Detailed Link):
 
Example 6: Non-Linear Order Cursor Display
Direct YouTube link: https://youtu.be/MGRSnxU61oM
Highlights (with Detailed Link):

Note that there are custom displays created in both Simcenter Testlab and Simcenter Testlab Neo.  Here are instructions for creating custom displays in both software packages: Questions or comments?  Email peter.schaldenbrand@siemens.com or charles.rice@siemens.com. 

Related Links:

Powered by