Salesforce

Quick Start Guide to SCADAS RS Hardware

« Go Back

Information

 
TitleQuick Start Guide to SCADAS RS Hardware
URL NameQuick-Start-Guide-to-SCADAS-RS-Hardware
Summary
Details


Direct YouTube link: https://youtu.be/OJ9Mc7cMgb0



This article explains how to get started with Simcenter SCADAS RS hardware.

Items covered include how to connect and power up the SCADAS RS hardware, connect to the onboard Simcenter SCADAS RS Recorder App, and how to connect to a PC to use with Simcenter Testlab Neo.

Contents:
1.    Connect and Power Up
2.    Wireless Connection
3.    Wired Connection 
4.    Simcenter Testlab Neo
5.    Changing Password, Network Name, and IP Address


1. Connect and Power Up

Simcenter SCADAS RS hardware consists of different hardware modules.  They can be connected to each other by snapping the bottom of one unit to the top of another unit as shown in Figure 1:
 

User-added image
Figure 1: Typical minimum configuration of a SCADAS RS consists of three modules: Power (UPS), Recorder (REC) and conditioning (B24/S24/U12/TC20).

A typical configuration for a SCADAS RS consists of at least three hardware units:
  • UPS: A power supply unit
  • REC: The main brains or recorder unit
  • U12/B24/S24/TC20: A signal conditioning unit
If using a AC/DC power adapter for powering the configuration shown in figure 1, it must be plugged into the UPS. The UPS unit shown in Figure 2.
Check the user manual for more information about connecting the AC/DC power adapter for different configurations.

 
User-added image
Figure 2: The SCADAS RS UPS module provides power for the entire SCADAS RS system.
 
The power module will be connected in turn to the other SCADAS RS modules.  The UPS module provides power to them.  Every SCADAS RS module has 2 Power/Data ports for power on its right hand side when facing the module, see figure 3.
 Figure_1.png 

Figure 3: All SCADAS RS modules have 2 power/data ports on their right hand side. The output of the UPS power module (top) is connected to the power input of the REC module (middle) to power it.  In turn, the output of the REC module is connected to the power/data input of the conditioning module (bottom).

Using the single power button on the UPS module, all attached SCADAS RS units will be powered up.

The cable also transfers data in addition to power.  All data is synchronized and transferred to the SCADAS RS REC module where it is stored in a single file.

Multiple signal conditioning units (B24, S24, U12, TC20, etc) can be used with a single UPS and REC, but with a maximum of 4 units.  More information about SCADAS RS conditioning units and modules in the knowledge article: Simcenter SCADAS RS for Testing in Harsh Environments.

2. Wireless Connection

The Simcenter SCADAS RS has an embedded application called the Simcenter SCADAS RS Recorder App.  It can be run via a browser on any wireless devices as shown in Figure 4:

User-added image
Figure 4: Data can be acquired and viewed on the SCADAS RS using a web browser from any wireless device.

The SCADAS RS REC module has a built-in Wi-Fi network.  To connect wirelessly to the unit, attached both Wi-Fi antennas to the REC unit to the ports indicated in Figure 5:
 
User-added image
Figure 5: The SCADAS RS comes with two Wi-Fi antennas (right) that must be attached to the two ports on the REC module (left).

When the SCADAS RS is powered on and both antennas are present, any wireless enabled device will see a SCADAS RS-2G wireless network.  Like most Wi-Fi, connections are possible up to 150 feet or about 34 meters away.

After connecting to SCADAS RS wireless network (password SCADAS-RS), use a web browser to navigate to the IP address of the REC (default: 100.123.10.1). 

*** Note: The default password and network name can be changed to help secure the data acquisition system.  See upcoming section for instructions on how to do so. ***

If this is the first time connecting, a login and password for the device must be entered (this is in addition to the wireless network connection with password) as shown in Figure 6:
User-added image
Figure 6: Username and password prompt for the SCADAS RS Recorder App.

The default login and password are:
  • User: USER or ADMIN
  • Password: “SCADAS-RS”

After logging in, the Simcenter SCADAS RS Recorder App appears as shown in Figure 7:
 
User-added image
Figure 7: Simcenter SCADAS Recorder App (left) for SCADAS RS hardware (right).

More about using the SCADAS RS Recorder App in the knowledge article: Simcenter SCADAS RS Recorder App.

3. Wired Connection

It is also possible to connect to the SCADAS RS with a hard wired ethernet connection.  An example using a PC is shown in Figure 8:
 
User-added image
Figure 8: Example of a wired ethernet connection between PC and SCADAS RS.

Both the embedded SCADAS RS Recorder App or Simcenter Testlab Neo can be used with the SCADAS RS hardware in a hardwired configuration.

To use a wired connection, attach the ethernet cable to the “1Gbe” port on the SCADAS RS REC unit as shown in Figure 9:
 
User-added image
Figure 9: The SCADAS RS ethernet cable (left) has a regular CAT 6 connection on one end and a ruggedized connector on the other.  The ruggedized connector is plugged in the “1GbE” port (second from the left on the bottom row) of the REC unit.

By default the SCADAS RS will be set on a dynamically allocated IP address, a fixed IP address can be set in the app. For instructions on configuring the host PC to use a dynamically allocated IP address, please refer to the attached guide in this article.

Some evaluation SCADAS RS units ship with a fixed IP address of 192.168.2.172 (if not a dynamic allocation).  In this case, set the IP address of the PC ethernet card to 192.168.2.1.
 
Two ways to open the Simcenter SCADAS RS Recorder App on the host PC:
  • If the IP address of the SCADAS RS Recorder is known (for example 192.168.2.172), enter this IP-address in the address bar of the web browser. 
  • Go to Windows Explorer-Network and double click on the SCADAS RS Recorder device in Other devices section. ( see the attached guide in this article)

The Simcenter SCADAS RS Recorder App will appear (login may be needed) as shown in Figure 10:
 

User-added image
Figure 10: Simcenter SCADAS RS Recorder App main menu.

The SCADAS RS Recorder App is used to:
  • Setup analog data acquisition channels (including name, power supply, etc)
  • Setup digital channels including CAN bus and digital IO 
  • Calibrate transducers
  • Record data including defining triggers to automatically start and stop the measurement
  • View time history data
  • Download data to a local PC for further processing

More about using the SCADAS RS Recorder App in the knowledge article: Simcenter SCADAS RS Recorder App

4. Simcenter Testlab Neo

With a hard wired ethernet connection, it is also possible to use Simcenter Testlab Neo software to acquire data from the SCADAS RS to the host PC (Figure 11):
 
User-added image 
Figure 11:  Simcenter Testlab Neo connected to SCADAS RS.

Simcenter Testlab Neo has two different applications that can work with the SCADAS RS:
  • Time Data Acquisition: Required license, records data to host PC  
  • Recording Workbook: No license needed, setup only and cannot acquire data

Go to the folder “Simcenter Testlab Neo General Acquisition” or search windows to find these programs.

Double click on either Simcenter Testlab Neo programs.  New template and frontend selection prompts are shown in Figure 12:
 
User-added image 
Figure 12: Startup of Neo acquisition prompts for templates and frontend hardware selection.

In the new template selection, Do NOT click on “Work Offline”.  In the Hardware selection menu, select SCADAS RS, enter IP address, login: USER, password: SCADAS-RS.

4. Changing Password, Network Name, and IP Address

For added security, the default password, network name, and IP address can be changed using the Simcenter SCADAS RS Recorder App.  From the main menu of the Recorder App, select the “Topology” icon as shown in Figure 13:
 
User-added image
Figure 13: Select “Topology” icon from main Simcenter SCADAS RS Recorder App.

To change the Wi-Fi password, click on the triple dot button on the right side of the screen and select “Password Manager” as shown in Figure 14:

User-added image 
Figure 14: To change the Wi-Fi password, click on the triple dot button on the right side of the screen and select “Password Manager”.

Enter a new password.

To change the Wi-Fi network name, click on the triple dot button on the right side of the screen and select “Wi-Fi settings” as shown in Figure 15.
 
User-added image 
Figure 15: To change the Wi-Fi network name, click on the triple dot button on the right side of the screen and select “Wi-Fi settings”.

To change the IP address, click on the triple dot button on the right side of the screen and select “Network settings” as shown in Figure 16 below.
 
User-added image  
Figure 16: To change the SCADAS RS IP address, click on the triple dot button on the right side of the screen and select “Network Settings”.

The network can be set to a fixed IP address or to a dynamically allocated IP address (also called DHCP).

Powered by