Salesforce

Gallery of Simcenter Testlab Neo Processes

« Go Back

Information

 
TitleGallery of Simcenter Testlab Neo Processes
URL NameGallery-of-Simcenter-Testlab-Neo-Processes
Summary
Details
The Simcenter Testlab Neo Process Designer is used to create custom step-by-step analyses that can encompass multiple steps as shown in Figure 1:
 
User-added image
Figure 1: A Simcenter Testlab Neo process consists of multiple connected methods that automate a data analysis.

Processes can encompass multiple functions including:
  • Processes can start with raw time data and/or spectrums/orders/FRFs etc
  • Data can be conditioned including filters, detrending, segmenting
  • Processing options include spectrums, FRFs, orders, statistics.
  • Output options include Excel, Powerpoint, etc.
*** The processes described in the next sections are in a zip file attached to this article. ***


This article has example videos and highlights of several different processes:
   1. Process Basics
   2. Calculating and Comparing Orders and Overall Levels
   3. Averaging Multiple Channels with Block Calculator
   4. Modulation Metrics
   5. Data Validation
   6. Rosette and Critical Plane Analysis
   7. Early Detection of Bearing Faults
   8. Damage-based Time Compression
   9.  Anomaly Detection
   10.  Human Body Vibration
   11. Exporting Processed Results to Excel



1. Process Basics

The Process ribbon in Simcenter Testlab Neo Process Designer contains icons for opening already created processes as well as creating new ones (Figure 2):
 
User-added image
Figure 2: The ribbon in the Simcenter Testlab Neo Process designer allows processes to be created, opened, and saved.

The ribbon creates and opens process files with a *.process extension.  These files contain all pertinent methods and connections and can be shared with other users.

More about Simcenter Testlab Neo Process Designer in the knowledge article: Simcenter Testlab Neo: Process Designer.

2. Calculating and Comparing Orders and Overall Levels over Multiple Runs

Direct YouTube link: https://youtu.be/9-_AYpVe1_8

In this process, raw time data with rpm data is processed into orders and overall levels.  Averages are calculated over multiple runs. Key methods include Spectral Map, Orders Sections, Overall Level, and Run Average (Figure 3).
 
User-added image
Figure 3: Simcenter Testlab Neo Process that calculates order, overall level and averages over multiple runs.


More details in the knowledge article: Calculating and Comparing Orders and Overall Levels in Simcenter Testlab Neo

3. Averaging Multiple Channels with Block Calculator

Direct YouTube link: https://youtu.be/wzVIwA0rZ_o

This process shows how the spectrums of multiple channels can be averaged together.  Different means (selecting specific channels versus using wildcards *) for selecting the data are shown with the Block Calculator method.

More information in the knowledge article: Simcenter Testlab Neo: Combined, Block Calculator, and Signal Generation Methods

4. Modulation Metrics

Direct YouTube link: https://youtu.be/VkZtUiYSH7k

In this process, the amount of modulation (periodic rising and falling in level of a signal) is evaluated using several different methods: "Envelope", "Modulation Spectrum", "Modulation Map", and "Modulation Depth".  The human response to modulation is also calculated using "Fluctuation Strength" and "Roughness" methods.

More details in the knowledge article: Simcenter Testlab Neo: Modulation Metrics

5. Data Validation

Direct YouTube link: https://youtu.be/9-_AYpVe1_8

In this process, an automotive braking data validation process is explained in detail.  In this case, specific data is extracted by creating an "Index channel" (has a value of 0 or 1 depending on criteria applied versus time) using the "Calculate" method.  The "Decompose" method is used to reassemble the extracted data for further processing.  Statistics are then calculated from the extracted data.

More information in Siemens Simcenter Blog: Stopping power: Improving brake performance testing with advanced DAQ and data validation software

6. Rosette and Critical Plane Analysis

Direct YouTube link: https://youtu.be/Idmn8b6ZuKk

Simcenter Testlab Neo Process Designer has multiple ways to analyze measured strain gauges.  This process shows how to use the "Rosette" and "Critical Plane" methods.

More information in the knowledge article: Rosette Strain Gauges

7. Early Detection of Bearing Faults

Direct YouTube link: https://youtu.be/nSSgxGQzOwc

The "Envelope" method helps gain early insight into bearing failures (Figure 4).

User-added image
Figure 4: The "Envelope" method is used to help identify early failures in bearings.


More information in the knowledge article: Early Detection of Bearing Faults using Simcenter Testlab

8.  Damage-based Time Compression


Direct YouTube link: https://youtu.be/_AGXQnaJH4U


To decrease the amount of time it takes to perform a durability test, it is possible to remove small amplitude fatigue cycles (that do not create large amounts of damage) from a time history. A new condensed time history that has close to the original amount of damage potential can then be used to perform the durability sign-off test in a condensed amount of time (Figure 5).
 

User-added image
Figure 5: The original time history (top, red) is condensed (top, green) but still preserves 80% of the damage potential (green lower right) versus the original damage (red lower right).
 

This process also has settings that help preserve the frequency content as well.

More information in the knowledge article: Some Thoughts on Accelerated Durability Testing

9.  Anomaly Detection

Direct YouTube link: https://youtu.be/tGef1mYYfUc

During data collection many potential "anomalies" can occur. Sensors can come loose and fall off of their intended measurement locations.  Electro-magnetic interference can induce electrical noise in the measured data.

Spikes and drift can also occur in data (Figure 6).

User-added image
Figure 6: Top: Spikes/dropouts are one type of anomaly that can occur. Bottom: Offsets can occur in sensor reading over time creating drift.

It can be very tedious and time consuming to inspect hours of recorded data over hundreds of channels.  The anomaly detection process helps flag potential measurement issues in an automated way.

More information in the knowledge article: Simcenter Testlab Neo Anomaly Detection

10.  Human Body Vibration

Direct YouTube link: https://youtu.be/vBwyIiIL_m0


Simcenter Testlab Neo Process Designer includes processes for:

  • ISO 2631: Whole Body Vibration
  • ISO 5349: Hand Arm Vibration

These processes are used to take vibration measured at human interface locations (seats, steering wheels, drill handles, etc) and predict either human comfort or exposure limits.

More information in the knowledge article: Human Body Vibration

11.  Exporting Processed Results to Excel

Direct YouTube link: https://youtu.be/HyJqu_lhGPg


This process highlights how both measurement functions (spectrums, etc) and statistics can be exported to Excel in Simcenter Testlab Neo Process Designer (Figure 7).

User-added image
Figure 7: Simcenter Testlab Neo process with "Report to Excel" method.

The "Report to Excel" method is used in these processes.

More information in the knowledge article: Import/Export Data between Excel and Testlab


Questions?  Email scott.beebe@siemens.com. 

Related Links:

Powered by