Salesforce

Simcenter Testlab Neo and Video

« Go Back

Information

 
TitleSimcenter Testlab Neo and Video
URL NameSimcenter-Testlab-Neo-and-Video
Summary
Details

Direct YouTube link: https://youtu.be/sxJ3wJreATI


Simcenter Testlab Neo has multiple options to support data acquisition with synchronized video (Figure 1).
 
User-added image
Figure 1: Example video playback synced with analog data from vehicle.
 
Options include acquiring video synced with analog data channels (strain, vibration, etc), video playback, and importing video for post analysis.

This article covers the following:
   1. Video Acquisition:
      1.1 USB Camera and PC
      1.2 SCADAS RS 
      1.3  Supported Cameras
      1.4 CIM2 and SCADAS
   2. Video Replay
      2.1 Video Viewing
      2.2 Imported Video and Sync


1. Video Acquisition

There are several options to collect video data simultaneously with analog data channels (strain, acceleration, sound, etc).  

1.1 USB Camera and PC

To record video, a specific USB camera can be plugged into a laptop or PC that has Simcenter Testlab Neo Time Data Acquisition installed. See upcoming section for supported USB camera models.

Both Simcenter SCADAS data acquisition hardware (Ethernet or USB) and a video camera (USB) are connected to the PC as shown in Figure 2.
 
User-added image
Figure 2: PC with Simcenter Testlab Neo Time Data Acquisition configured with video camera and SCADAS hardware.

With the video camera plugged into the USB port of the PC, start Simcenter Testlab Neo Time Data Acquisition.

In the “Channels” view of the “Instrumentation” tab, the camera should be the last line in the channel list as shown in Figure 3.
 
User-added image
Figure 3: In the “Channels” tab of “Instrumentation”, turn on video camera with checkbox in channel list, select the “Camera Preview” from the home ribbon, and arm the system to verify camera is working.

Turn on the camera by clicking in checkbox at the beginning of the row. In the “Home” ribbon, turn on “Camera Preview” (icon on right side of ribbon) to open the camera preview area.

In order to check the image, arm the system and a live video feed should appear.

If the camera preview shows a image and is working, disarm and go to the “Measure” tab to take measurements and record video (Figure 4).
 
User-added image
Figure 4: “Measure” tab of Simcenter Testlab Neo with video capture.

Both data channels and video can be viewed while acquiring data.  Select data to view by clicking in the pivot table of the “Data Selection” area.

USB based video acquisition is available in version 2506 and higher of Simcenter Testlab Neo. Video recording only works with the specific USB cameras listed in Section 1.3 of this article.

1.2 SCADAS RS

Video capture with SCADAS RS hardware is also supported as described above, but SCADAS RS hardware is often used without a PC.

If no PC is present, there are USB ports on the SCADAS RS REC unit that can be used for collecting video (Figure 5).
 
User-added image
Figure 5: USB ports on the SCADAS RS REC unit that can be used for video inputs.

To connect a video camera to the SCADAS RS Rec unit, use a USB2 to Yamaichi cable (part number SCRSA-CAB004) or a USB3 to Yamaichi cable (part number SCRSA-CAB007).

Video can be captured using the Simcenter SCADAS RS Recorder App that is built into the SCADAS RS hardware (Figure 6). 
 
User-added image
Figure 6: SCADAS RS configured for acquiring video with Simcenter Testlab Recorder App.

In the SCADAS RS Recorder App, video can be viewed in the Monitor area.  There is a “Video” tab.  In the “Custom” tab video and data channels can be displayed together as shown in Figure 7 below.
 
User-added image
Figure 7: In the Monitor area of the Simcenter Recorder App a custom display can show data and video simultaneously.

Cameras that have been tested and work are described in the next section.

1.3 Supported Cameras

The following USB cameras are the only cameras tested and guaranteed to work with the SCADAS RS, SCADAS Mobile/Recorder, SCADAS XS, and with Simcenter Testlab Neo Time Data Acquisition with a PC:
  • Siemens ruggedized USB camera (Product code SCRSA-CAM0001) with 1920x1080 resolution, 120 degree field of view, 30 frames per second, IP69K protection.  Contact your Siemens sales representative worldwide.
  • Deepwater Exploration ruggedized USB camera (SKU/Product code DWE-CUSCAM-002) with 1920x1080 resolution, 120 degree field of view, 30 frames per second, IP69K protection. Contact "sales@dwe.ai". This camera is not on Deepwater website and is only available via special order. This is for customers located in the United States.
User-added image
Figure 8: Siemens SCRSA-CAM0001 USB Camera
 
These video cameras are UVC (USB Video Class) compliant and support H.264 video compression. Due to the large variation in USB based cameras, only the cameras listed above are guaranteed to work with Simcenter Testlab Neo.

1.4 CIM2 and SCADAS

Another option to record video with Simcenter Testlab Neo Time Data Acquisition and SCADAS Mobile/Recorders is to equip the SCADAS with a CIM2 camera card. 

The video cameras will be connected to the CIM2 card in the SCADAS rather than to the PC.  A SCADAS Mobile/Recorder with CIM2 card is shown in Figure 9 below.

User-added image
Figure 9: SCADAS Recorder/Mobile equipped with CIM2 card.

Cameras are powered from SCADAS via POE (Power Over Ethernet).  These cables and cameras are provided with the CIM2 card.

The CIM2 card cameras work with Time Data Acquisition and in  standalone SCADAS Recorder mode. Standalone SCADAS Recorder mode is useful for scenarios where video recording is desired, but no laptop with Simcenter Testlab Neo is available.

See the Siemens support center for information on setup of CIM2 card (product code: SCM-CIM2) and cameras.

2. Video Replay

In the Simcenter Testlab Neo Desktop, recorded video can be played back along with recorded analog data channels.  This can be even be done with video data that was not originally recorded along with the analog data channels. 

2.1 Video Viewing

Turn on “Video Replay” under File -> Add-ins.  Then highlight the run that contains video data (Figure 10).
 
User-added image
Figure 10: Video replay is possible in the Simcenter Testlab Neo Desktop.

In a pivot table view, select the channels to view during replay including the video.  Use the play button to watch the data.  Press pause will stop the replay and the blue playback cursor can be manually moved.

Video replay can sync with both GPS and audio data.  To hear audio, turn on “Audio Replay” and “Advanced Audio Replay” under “File -> Add-ins”.

When not in replay mode, add a coupled cursor (“Right click -> Add Coupled Cursor -> Throughput”) in the display to manually advanced back and forth in the video and data channels. 

2.2 Imported Video and Sync

MP4 video files that were acquired separately can be imported for playback.

Importing video is useful when it was not acquired through synchronized means as described previously in this article. After import, the video can be synced with the analog data acquisition channels.

Right click on the run containing the analog channels and choose “Import” and select a *.mp4 file a shown in Figure 11.
 
User-added image
Figure 11: To import an external video file into Testlab Neo, right click on the run, select “Import” and select a MP4 file. 
 
 After importing the data, the mp4 can be synced with the analog data channels with the Video Sync feature. (Figure 12).
 
User-added image
Figure 12: An imported mp4 file can be synced with analog data channels.

This is done by aligning on a common event in both the video and the data.

For detailed information on the Video Sync feature, see the knowledge article: Importing Video in Simcenter Testlab Neo


Enjoy!  Questions?  Email scott.beebe@siemens.com. 


Related Links:

Powered by