Salesforce

Cool Channel Setup Tricks for Triaxial Accelerometers

« Go Back

Information

 
TitleCool Channel Setup Tricks for Triaxial Accelerometers
URL Namecool-channel-setup-tricks-for-triaxial-accelerometers
Summary
Details


Direct YouTube link: https://youtu.be/p1EvCVzmwGk
 

User-added image
Looking to setup triaxial accelerometers quickly and correctly in Simcenter Testlab? 

If so, here are three tips for you!:

1. Use Auto Fill

In the Simcenter Testlab (formerly LMS Test.Lab) "Channel setup" worksheet, highlight the PointId and Direction of a triaxial accelerometer. Hover the mouse in the lower right hand corner of your selection.

4-9-2016 9-58-42 AM.png

Hover mouse in lower right corner of triaxial selection until double white arrow appears

Once a Double White arrow appears, drag the mouse down or up to fill in the other channels. The "PointId" field will be automatically incremented, and the "Direction" fields will be filled with the same information as the original triax information.

4-9-2016 9-58-11 AM.png
Drag the arrow up/down with the mouse to auto fill triaxial information on the other channels

2. One Wire Triaxial Accelerometers

If you use a Simcenter SCADAS V-24 card or SCADAS XS, you can connect a 3 channel triaxial accelerometer with one cable.


Triaxial_cable.png

Single cable triaxial accelerometer and SCADAS XS

For example, if you have a PCB Triaxial Accelerometer (either 4 pin or mini 4 pin), you can order PCB cables:

  • PCB Cable 010M136/M003 (SCADAS Lemo to 4 pin connector) where the "003" means 3 meters (5 and 10 can be substituted for the "3")

OR

  • PCB Cable 034M59/M003 (SCADAS Lemo to 4-pin miniature connector)

 

XS_Triax2.jpg
SCADAS XS and SCADAS V-24 lemo connection support single cable connections for triaxial accelerometers

Compared to a traditional 3 BNC connection, this makes it impossible to cross wire the triaxial directions!

3. Enforce Right Hand Rule Automatically

By default, directions on channels can be set independently. Directions are not checked for compliance to the right hand rule. This can lead to mistakes when doing a Modal Analysis or Operational Deflection Shape.

triax3.png
Default Channel Setup behavior allows directions to be set independently on each channel

In Tools -> Channel Setup Visibility, add the channel setup field called "MultiChannel". For any triaxial accelerometer channels, set the "MultiChannel" value to "Triax-RH".

User-added image
Setting "MultiChannel" to "Triax-RH" limits direction selections to valid right hand rule combinations

Setting a group of three channels to "Triax-RH" limits the selection of directions to valid Right Hand Rule combinations. No more "flyer points" on Modals and Operational Deflection Shapes!

Hope these tips help!

PS> If you are from Australia, there is a "Triax-LH"....  



See the knowledge article Simcenter Testlab Data Acquisition Tips for even more information on channel setup and other data acquisition options.

If you have questions, feel free to email peter.schaldenbrand@siemens.com or contact Siemens Support Center.

 

Related Simcenter Testlab acquisition tips:

Other Articles:


Powered by