Salesforce

Simcenter SCADAS RS: Assorted Tips and Tricks

« Go Back

Information

 
TitleSimcenter SCADAS RS: Assorted Tips and Tricks
URL NameSimcenter-SCADAS-RS-Assorted-Tips-and-Tricks
Summary
Details
User-added imageThis article contains assorted tips on using Simcenter SCADAS RS hardware with both the Simcenter SCADAS RS Recorder App and Simcenter Testlab Neo.

Tips include:
1. Custom Displays
2. Zero Before Acquisition
3. Digital IO
4. Creating a Template
5. SCADAS RS Configuration Builder
6. SCADAS RS Schedule Designer and Export Tool
   6.1 Schedule Designer
   6.2 Download and Export Tool



 
1. Custom Displays

The Simcenter Testlab Recorder App has built-in strip chart and statistic displays that are active during acquisition.  These built-in displays show all channels in a predesigned display.  These displays are found in the “Monitor” section of the Recorder App.

However, custom displays can be created as well.  This is done in the last tab of “Monitor” as shown in Figure 4:
 
User-added image
Figure 4: In the “Custom” tab (right most tab in “Monitor”) users can create custom displays.

Gauge displays, XY displays, numerical displays are available in the custom display area.

2. Zero Before Acquisition

Direct YouTube link: https://youtu.be/M9UtYL5ZIW8


When taking strain measurements, it is a common practice to “zero out” strain channels before starting a measurement.

It is possible to setup the SCADAS RS to automatically zero channels at the start of any acquisition. To set this up, click on "Recording Setup" from the main menu of the Simcenter SCADAS RS Recorder App as shown in Figure 1.
 
User-added image
Figure 1: From the main menu of the Simcenter SCADAS RS Recorder App, select "Recording Setup".

In the “Recording Setup” section, “Auto zeroing” can be turned ON as shown in Figure 2.
 
User-added image
Figure 2: Turning on “Auto zeroing” in the Recording Setup.

The measurement might contain several channels of non-strain data. So not all channels should be zeroed.

In this case, it is possible to exclude certain channels from being automatically zeroed.  This is done in the “Offset Calibration” section of the software as shown in Figure 3.
 
User-added image
Figure 3: In the “Zeroing” column, select which channels should be zeroed.
 
Using the “Zeroing” column, channels can be toggled on and off based on whether they should be zeroed or not.
 
3. Digital IO

On the main unit (REC unit) of the SCADAS RS, there is Digital Input and Output ports a shown in Figure 5.
User-added image
Figure 5: A four channel digital input and output port is located on the SCADAS RS REC unit.

The digital output can be used to send out a voltage signal when levels are exceeded on a channel, at the end of an acquisition, etc.

In the “Recording Setup”, there is a tab called “Digital IO” where the outputs on the four different digital input output port pins can be defined as shown in Figure 6.
 
User-added image
Figure 6: Setup menu for Digital IO port.

The Digital IO setup can evaluate many different conditions as shown in Figure 7.
 
User-added image
Figure 7: Setup menu for conditions that trigger can be evaluated. 

The Digital IO feature can be used to trigger the shutdown of a test stand if vibration becomes too high, etc.

4. Templates

Templates are setup files that contain all the information needed to run a test.  This includes channel information, trigger settings, and acquisition settings.

After setting up a test measurement, all the settings can be stored in a template. Templates are managed in the “Topology” and “Templates” icons of the main menu of the Simcenter Testlab Recorder App (Figure 8 below).
 
User-added image
Figure 8: Both the “Topology” and “Template” icons are used to manage measurement templates.
 
To create a template of the current active measurement settings, click on the “Topology” icon.

In Topology area, click on “Save As” on the left side of the screen as shown in Figure 9.
 
User-added image
Figure 9: Click on “Save As” to create a template with the current measurement settings.

After clicking “Save As”, fill in the template name and press the “Save” button. Press the back arrow (upper left) to go to the main menu.

To activate a saved template, from the main menu, click on the “Templates” icon.  A list of all available templates should appear on the screen (Figure 10):
 
User-added image
Figure 10: List of available templates.

At the bottom of the template, press the “Load Template” icon to activate the settings.

5. SCADAS RS Configuration Builder

Want to setup a test template for the SCADAS RS, but don’t have the hardware?  

Create a frontend configuration file (*.nfec) that can be used to set up a test without being connected to actual hardware using Simcenter Testlab Neo.

In the Windows search area, look for “scadas rs”.  Start the “SCADAS RS Configuration Builder” as shown in Figure 11:
 
User-added image
Figure 11: Search for “scadas rs” in Windows to start the “SCADAS RS Configuration Builder” utility.

In the SCADAS RS Configuration Builder, acquisition modules can be dragged from the library on the right to the measurement chains on the left as shown in Figure 12.
 
User-added image
Figure 12: In the SCADAS RS Configuration Builder, move conditioning units from the library on the left to the measurement chain on the right.

A UPS and REC unit are already active by default.

Press the “Save” button (top row) after finalizing the hardware selection.  The SCADAS RS hardware configuration will be stored in a *.nfec file. Exit the program after saving the file.

When starting Simcenter Testlab Neo acquisition, if selecting work offline mode, the *.nfec file can be selected as shown in Figure 13.
 
User-added image
Figure 12: Using a *.nfec file in offline mode of Simcenter Testlab Neo acquisition.

6. SCADAS RS Schedule Designer and Export Tool

Direct YouTube link: https://youtu.be/uqXhf2ZFFJw


Two accompanying software packages for the SCADAS RS are the "Schedule Designer" and the "Download and Export Tool".

6.1 Schedule Designer

The SCADAS RS Schedule Designer (released with SImcenter Testlab 2506 and higher) is a no additional cost add-on for that works Simcenter SCADAS RS. It is a PC based application that allows a set of pre-defined tests to be identified for execution (Figure 13):
User-added image
Figure 13: The standalone PC-based SCADAS RS Schedule Designer software allows a sequence of tests to be defined.  In this case, the tests are called: "Run-up", "Constant speed 30 kph", "Constant speed 50 kph", and "Constant speed 80 kph". 

For example, four tests with different conditions could be defined: "Run-up", "Constant speed 30 kph", "Constant speed 50 kph", "Constant speed 80 kph". These are called "tasks". Each task has a unique channel setup and test parameters (triggers, duration, etc), and user prompts.

Once the schedule of tests or tasks are defined, the schedule is transferred to the SCADAS RS hardware to be used with the SCADAS RS Recorder App.

In the SCADAS RS Recorder App the schedule is loaded. The Recorder App will prompt for each test to be performed (Figure 14):
 
User-added image
Figure 14: With a schedule of tests defined, the SCADAS RS Recorder App prompts for each test to be executed and saved. Tests can be also be defined with an auto-save.

When running the schedule, the SCADAS RS Recorder App will track the tests that have been completed.  It will guide the user for which tests are to be performed next.  A running status is shown.

6.2 Download and Export Tool

A PC based software that is included in the SCADAS RS Recorder App is the "Download and Export" tool (Figure 15).
 
User-added image
Figure 15: The "Download and Export" tool is used to quickly batch download files from the SCADAS RS and export to other file formats.

The software can be downloaded from the SCADAS RS Recorder App and installed on a local PC.  After installing and connecting to the SCADAS RS, files can be download and export to several different file formats.
 

Hope these SCADAS RS tech tips are useful!

Questions?  Email nicholas.divincenzo@siemens.com.

Related Links:

Powered by