Salesforce

Simcenter Testlab 2606: Download and Install Instructions

« Go Back

Information

 
TitleSimcenter Testlab 2606: Download and Install Instructions
URL NameSimcenter-Testlab-2606-Download-and-Install-Instructions
Summary
Details
Simcenter Testlab 2606: Download and Install Instructions


This article covers how to download and install Simcenter Testlab 2606 software. Simcenter Testlab 2606 was released in July of 2026.

Article contents: 
1.    Downloading the Simcenter Testlab software
2.    Installing the License Server
3.    Installing the Simcenter Testlab software
3.1.    Preparing Installation
3.2.    Installing Prerequisites
3.2.1.    Installing the Configuration and Unit System
3.2.2.    Installing Hardware Diagnostics
3.3.    Installing Simcenter Testlab
4.    Installing Documentation
4.1     Installing the Documentation Server

4.2     Installing the Documentation Manuals
5.    Download and Installation of 1D and 3D Drivers
5.1.    Downloading Drivers
5.2.    Installing Drivers

1. Downloading the Simcenter Testlab Software


Direct YouTube link: https://youtu.be/ruLXiRVJqWg


First download the software from the Siemens Support Center:

 

  • If you have not accessed the Support Center before, you can do so through the Community Center, https://community.sw.siemens.com. Use the "Support" drop-down to navigate to the Support Center; you will be directed to log in if you are not already signed in.
Logging into the Support Center

 

  • In the Support Center, click on "Simcenter Testing Solutions" under the "Downloads" dropdown menu as shown below:

 

Locating Simcenter Testing Solutions  
 
  • Click on the "Simcenter Testlab 2606" release from the available options.  If it does not appear, select "All Versions" or "Simcenter Testlab 2606" from the "Select a Version" dropdown menu.

 

Locating the Simcenter 2606 Downloads

 

  • Click on "Simcenter Testlab 2606" from the tree on the left, and download the "Simcenter Testlab 2606.iso" file.

 

Downloading the 2606 iso file


A ISO file is a single file that contains all the installation files.  An ISO file is an "Image" file that can be burned to a DVD if desired.  However, it is not necessary to burn it to a DVD to install it.  It can be installed directly from the ISO file on a PC.  See the instructions below for how to do this.

More information about ISO files can be found here: https://en.wikipedia.org/wiki/ISO_image

2. Installing the License Server

If installing Simcenter Testlab on a network with access to a central license server, it is not necessary to install the License Server on the local machine.  Skip ahead to section 3.

If the license will be local to the PC, the license server software needs to be installed.  See the article Simcenter Testlab: RLM License Server 17.1 Installation and Setup for more information.

3. Installing the Simcenter Testlab Software


Direct YouTube link: https://youtu.be/Or7MXDRoqYo


After the software has been downloaded, the installation can start.

3.1 Preparing Installation

Using the ISO file in Windows file explorer:

To extract the installation files from the ISO file:

  • In Windows 10 or Windows 11, right click on the iso file and select Mount. 
  • In Windows 7, right click on the iso file and unzip it using WinZip, 7zip, or another extracting software.

After extracting or mounting the files, several directories and an "autorun.exe" file should be available as shown below.

Right click on the file that says “Autorun.exe,” and select “Run as Administrator.” You need full administrator rights on your computer to install.
 

Running autorun.exe as administrator
 

The main installation menu should appear. Select the top option, “Install Simcenter Testlab,” to begin the installation. 

The main Testlab Installation window
 
     
    If a popup window appears that says some prerequisites are needed to run the software, click "Next" to view or change the prerequisite components that will be installed or upgraded.
     
    The Prerequisites Setup Wizard

    The prerequisite step checks if certain libraries and other needed programs are present on the computer for Simcenter Testlab to run successfully.
     
    • Click "Next" to begin the installation of the items that are checked.

    The prerequisites selection page.

    3.2.1 Installing the Configuration and Unit System


    The Simcenter Configuration and Unit System tool is used to manage the preferred quantity units, as well as the folder locations for user and group settings.
     

    The installation wizard of the Simcenter Configuration and Unit System.

    • When designating a root location for user configuration settings, be sure to use a location with both read and write access.  Each user will get their own subfolder, and will need to be able to interact with that location.

    Selecting a directory for configuration settings.

    • If desired, a location shared with other users can be designated as a group configuration folder.  This can be useful for standardizing custom settings such as layouts, print templates, and processing settings.

    Choosing a group folder.

     

    • Click “Finish” on the last screen to move to the next part of the Simcenter Testlab installation.


    3.2.2 Installing Hardware Diagnostics

    The pop-up window for the Simcenter Hardware Diagnostics will come up. This utility is used to scan Simcenter SCADAS hardware and make a diagnostic report.

    • Click "Next" to start the installation.
    The Hardware Diagnostics Wizard
    • Click “Next” through the installation to choose all default settings, until you reach a window asking if you want to install the Simcenter SCADAS XS driver. Check this box. This will ensure proper installation of the XS driver for current or future use. Select next.
    Selecting the SCADAS XS driver
    • On the next screen, keep the default option to enable the exceptions to the Windows firewall during the installation. Select "Next."
    Enabling Firewall Exceptions
    • Select "Install" to begin the installation of the Simcenter Hardware Diagnostics; once complete, click on "Finish" to move on to the installation of Simcenter Testlab.

    3.3 Installing Simcenter Testlab

    Now the main part of Simcenter Testlab will be installed.
    • Click “Next” through the installation to choose all default settings.
    Main window of the 2606 Installation Wizard


    Certain functionalities of Simcenter Testlab use the Microsoft ODBC driver; since the 2606 release is 64-bit, these features may not work if the 32-bit version of the Microsoft ODBC driver is installed.  To determine how or whether to switch drivers, please refer to the article Simcenter Testlab 2306 - Resolving ODBC data source issues caused by Microsoft Access Database Engine installation.
     

    Simcenter Testlab features that require the 64-bit ODBC driver


    When coming to the screen asking to fill in the license file or the license server, select the box “Use a license server.”

    • Local License Server: If using a local license (node-locked or dongle license), type localhost into the space provided.
    • Network License Server: If using a network license, type in the server name after localhost separated by a semicolon. The default port is 5053, which is already considered in the default localhost option.
    • If the IT department has a specialized port number for Simcenter Testlab software, add it in front of the server name (Example: portnumber@server or portnumber@localhost).
    • Select "Next."
    Selecting the Licensing Server

    For the help documentation, the software can be left at its default selection to use the online documentation manuals hosted by the Support Center without the need for any further installation.  However, if you want to direct it to instead use manuals from a specific Documentation Server that you have access to, you can enter the server hostname of the computer hosting that server and port number that was selected during the server's installation.  If you intend to install a Documentation Server onto your own computer for offline access to the manuals, keep the server name as "localhost" to indicate the computer itself, and ensure that the same port number is used here as when installing the Documentation Server.
     

    Selecting the source for the documentation manuals.

    On the next screen, choose Desktop – Standard or Desktop – Advanced based on the licenses on your sold-to. These features can be found in your license file. Click "Next."
     

    Selecting a version of Desktop

    Select "Install" to begin the installation; once the Simcenter Testlab installation is complete, click "Finish."


    Once Simcenter TestLab is installed, you will need to install the RLM License Server. The Simcenter Testlab: RLM License Server 17.1 Installation and Setup is covered in a separate article.
     
     
    If using the Support Center option for access to the manuals, no further installation of the documentation is needed.  However, if you intend to set up a Documentation Server for use by yourself or your team, you can install the help server and its manuals from the main page of the Simcenter Testlab installation wizard.
     
    The main page of the installation wizard.
     
     
    To install a local help server, begin by using the "Install Documentation Server" option from the main page of the Simcenter Testlab installation wizard.  The installation will begin with a language selection, which is for the installation wizard's interface itself, followed by options of where to install the Documentation Server and its shortcuts.
     
    The Documentation Server installation wizard
     
    When designating the port number, the application port is the number that users of the documentation server will need to enter on the documentation selection page of the Simcenter Testlab installation wizard.  If you are installing a documentation server for your own offline use and already installed Simcenter Testlab, use the same application port as what you had entered previously.
     
    Designating the application port
     
    If intending to serve the manuals to other users, the Documentation Server can be made accessible over the network.  Otherwise, it will be for use by only the local computer it is installed on, such as for offline access to the manuals.
     
    Determining whether to serve the manuals over a network
     
     
    After the Documentation Server has been installed, the contents of the manuals can be added to it using the "Install Simcenter Testlab manuals" option from the main page of the Simcenter Testlab installation wizard, or from the standalone download of the "docs-simcenter-testlab-2606-en-US.exe" from the same Downloads page as the .iso file.  These manuals can be used with existing Documentation Servers of version 3.2 or newer.
     

    Installing the offline manuals 

    5. Download and Installation of the 1D and 3D Drivers


    Direct YouTube link: https://youtu.be/cwWTS-ZK57o


    To utilize Simcenter Nastran, Simcenter 3D data, or Simcenter Amesim data in Simcenter Testlab, the following drivers need to be installed:

    5.1 Downloading Drivers

    In the Simcenter Testlab download section (see first section if needed) select "Simcenter Testlab Drivers" from the pulldown.
    Selecting the drivers
     
    • The option to download Simcenter 3D and Amesim Drivers will appear. To begin the download, simply click on the desired driver.
    Selecting a driver to install

    The Simcenter 3D Driver allows Nastran and other simulation mode shape and FRF files to be viewed in Simcenter Testlab.  See the knowledge article Nastran and Test: Compare Mode Shapes and FRFs for more information.

    The Simcenter Amesim Driver allows Simcenter Amesim models to be viewed and processed in Simcenter Testlab; more information is available in the knowledge article Accessing Simcenter Amesim Models in Simcenter Testlab for more information.  There are three versions of the driver available for download on the drivers page: the "Amesim 2604 and earlier" driver, which is compatible with Simcenter Testlab 2606; the "Amesim 2504 and earlier" driver, which is compatible with Simcenter Testlab 2506 and newer, and the legacy "Amesim 2022.1 and earlier" driver, which is compatible with older versions of Testlab such as Simcenter Testlab 2406; for more information, see the knowledge article Important information concerning supported Simcenter Amesim versions for the "Simcenter Testlab - Driver for Amesim".
     
    • Both the 1D and 3D .zip files will contain four files. Before beginning the install, make sure to extract the .zip folder to a safe location.
    Extracting the driver installer from the .zip file
     
    • Right click and run “Simcenter Driver Setup” for the desired driver as an administrator.
    Running the driver setup as administrator

     

    • The Simcenter Driver Setup will open. Click “Next” through the installation to choose all default settings.
    The driver installation wizard
    • Click “Install” once all default settings are selected.
    • Once completed, select “Finish”.
    The driver installation wizard


    Questions or issues? Please contact Siemens Support Center at the appropriate phone number listed on https://support.sw.siemens.com and have your sold-to number (sold-to is in license file, or choose Help -> About Simcenter Testlab from the software interface). The phone number for North America is 1-800-955-0000.

    See Simcenter Testlab: RLM License Server 17.1 Installation and Setup for information on how to install the RLM license server and set up your Testlab license file to complete the Testlab software setup.

    See Which files should I download for Simcenter Testlab 2606 for more information on the files and other product components available in the download area of Simcenter Testlab 2606.

    Have new Simcenter SCADAS hardware?  Check out the articles What’s in the box? Getting Started with Simcenter SCADAS and Getting Started with Simcenter Testlab.

    Other Simcenter Testlab Installation Resources:


    Powered by