Salesforce

Simcenter Testlab: The Versatile "Double X" Cursor

« Go Back

Information

 
TitleSimcenter Testlab: The Versatile "Double X" Cursor
URL Namesimcenter-testlab-the-versatile-double-x-cursor
Summary
Details


Direct YouTube link: https://youtu.be/8TGd6BhawHg



In Simcenter Testlab (formerly called LMS Test.Lab), the Double X cursor is a wonderful and powerful cursor for data analysis.

 

Double X: The Basics

To add a Double X cursor to a display, right click and choose “Add Double Cursor -> X” (Hint: Hold down the CTRL key when right clicking on the display to always get the cursor menu)

doubleX_add.png
Picture 1: Right click in display (press CTRL if needed) and "Add Double Cursor -> X"

On the Double Cursor, the left and right cursors can be moved (Picture 2):

  • Left Cursor: Moves both cursors together at the same time. The cursors stay fixed distance apart
  • Right Cursor: Moves only the right cursor, changes the distance between the two cursors

doubleX_move_cursors.png

Picture 2: Left cursor moves both cursors, right cursor changes width

Set the cursor to the frequency range desired to perform an analysis.

Double X: Max

Need the maximum over a frequency/rpm range? Want to know the frequency/rpm the max occurs at?

doubleX_max.png
Picture 3: Using the Double X cursor to find the maximum value in a frequency range

Right click on either the left or right of the Double Cursor and select “Calculations -> Max” (Picture 4).

doubleX_max2.png
Picture 4: Right click on the double cursor and choose "Calculations -> Max". Maximum will be displayed in a cursor legend.

The maximum appears in cursor legend, along with the frequency at which the maximum value occurs (Picture 5).

doubleX_max3.png

Picture 5: The maximum value and it's corresponding frequency will be shown in the legend.

Right click on the cursor legend and choose "Copy Values" to paste the maximum value into Excel.

Double X: Frequency Calculator

Looking at some time domain data and wondering what the frequency is present (Picture 6)?

time.png
Picture 6: Damped sine wave time history.

Right click on the Double X cursor and select “Calculations -> Freq (1/deltaT)” as in Picture 7.

time2.png
Picture 7: Determine the frequency of time data by selecting "Calculations -> Freq(1/T)"

Double X: Linear Regression

Trying to figure out your average acceleration from a RPM vs time trace (Picture 8)?

rpm_vs_time.png
Picture 8: RPM vs time data trace

 

To determine the rate of speed increase (ie, the acceleration) from the RPM vs time, right click on the cursor and choose "Calculations -> Linear Regression" (Picture 9).

rpm_vs_time2.png
Picture 9: To determine the rate of acceleration, right click and choose "Calculations -> Linear regression"

The "Linear regression" function fits a line to the data between cursors. The slope and offset of this line are displayed in the legend.

Right click on the legend and choose "Copy Values" to copy/paste the slope and offset to Excel.

Double X: RMS and Color

Want to know the RMS level over a specific frequency range?

rms.png
PIcture 10: Determining the RMS value of a frequency band within a spectrum

Right click on the Double X cursor and choose “Calculations -> RMS” as shown in Picture 11.

rms2.png
Picture 11: Right click on the Double X cursor and choose "Calculations -> RMS"

Want to highlight the frequency range of interest with a little pizazz? Add a bit of color by right clicking on the Double X cursor and selecting “Properties”.

color.png
Picture 12: Select a color for the Double X cursor

Turn on “Fill with color:” (Picture 12) and select some beautiful colors (Picture 13)!

rms3.png
Picture 13: Double X cursor with filled color

Even mix colors with overlapping frequency ranges!

rms4.png
Picture 14: Overlapping colors in dual Double X cursors

Questions? Email peter.schaldenbrand@siemens.com or contact Siemens Support Center.

 

More Simcenter Testlab Display Tips:


Powered by