Salesforce

What's New in Simcenter Testlab 2506

« Go Back

Information

 
TitleWhat's New in Simcenter Testlab 2506
URL NameWhat-s-New-in-Simcenter-Testlab-2506
Summary
Details
Simcenter Testlab 2506 is here! 
  • Simcenter Testlab 2506 was released in June 2025. "2506" is 25 for the year 2025 and 06 for the month of June.
  • Simcenter Testlab 2506.0001 (first service pack) was released November 2025.
  • Simcenter Testlab 2506.0002 (second service pack) was released March 2026.
  • Previous release was Simcenter Testlab 2406.

Check out the new features of Simcenter Testlab 2506 below:
 
ACOUSTICS 


Direct YouTube link: https://youtu.be/Ft_X9l1WbpM

New acoustic highlights of Simcenter Testlab 2506 include:
  • Simcenter Testlab Neo Sound Power
    • Supports both ISO 3744 and ISO 3745 (precision method): 
      • ISO 3745 K1 correction for background noise per channel or per average, ISO 3744 background noise average correction only
      • ISO 3745 K2 correction based on environmental condition (temperature, humidity, etc)
      • ISO 3745 is only available in Neo
    • Directivity analysis
    • Sound power maps
    • Frequency sections, octave sections, and overall level on sound power map
    • Simcenter Testlab Neo supports these calculations in 1/3 octaves (per standard) and narrowband autopower (for diagnosis)
  • Simcenter Testlab Neo Sound Quality
    • FFT Based Articulation Index added in addition to filter based Articulation Index
    • Sound Metric Map calculations (Prominence Maps, Tone-to-Noise maps, Loudness maps)
    • Pass-by Noise Testing
      • Wind speed data max over 10 recordings
      • Driver aid extensions
       User-added image
    Summary reports are among the extensions for the pass-by noise driver's aid.

     
    DURABILITY AND GENERAL ACQUISITION 

     
    Direct YouTube link: https://youtu.be/sxJ3wJreATI

    New durability and acquisition highlights include:
    User-added image
    Test scheduler in Simcenter SCADAS RS Recorder App.
       
     
    MODAL TESTING 


    Direct YouTube link: https://youtu.be/RJJSFperJhQ

    With Simcenter Testlab 2506, a new Smart Hit Selection in Simcenter Testlab Neo was introduced.
    User-added image
    When acquiring modal impact FRFs, Simcenter Testlab Neo not only rejects overloads and double hits, it will automatically select the hits that yield the highest coherence.
     
    MODAL ANALYSIS 


    Direct YouTube link: https://youtu.be/DLRUlJxnuOQ

    Simcenter Testlab 2506 features the release of Simcenter Testlab Neo Modal Analysis.  The selection of the modes is automated via a Artificial Intelligence (AI) algorithm.
     
    User-added image
    Simcenter Testlab Neo Modal Analysis has Artificial Intelligence (AI) powered mode selection.  After selecting the modes, the Modal Assurance Criterion and Modal Synthesis are automatically calculated.
     
    NEO PROCESS DESIGNER 


    Direct YouTube link: https://youtu.be/zz5fQwNBI3w

    New features in 2506 Neo Process Designer include:
    • Multi Reference Processing for FRFs and Crosspowers including SVD truncation and balancing
    • Additional map statistic methods (averaged and peak order spectrum)
    • Block methods in Simcenter Testlab Neo Process Designer: Import block method and Align X Axis Block method
    • Extensions to variables including conditions and Excel
    User-added image
    The use of variables in processes includes conditional usage of variables and support of Excel.

     
    TRANSFER PATH ANALYSIS 


    Direct YouTube link: https://youtu.be/ALVE7Plu6Fg

    New features in 2506 Transfer Path include:
    • Transfer Path Analysis in Neo:
      • Direct
      • Matrix Inversion
      • In-situ TPA for blocked forces
    • Dynamic mount stiffness calculator in Neo
    • Principal component multi-reference processing in Neo Process Designer
    • Noise simulator pre-processing including order extraction and coherent spectra processing (Neo Process Designer)
    User-added image
    Noise simulator capabilities are extended in the 2506 release to include decomposition methods.

    See the PDF attached to this article for a full description of the new features of Simcenter Testlab 2506.

     
    INSTALLATION 

    Download and installation: Simcenter Testlab 2506: Download and Install Instructions

    Past releases:

    Powered by