Salesforce

Order Tracking: Fixed Sampling versus Synchronous Sampling

« Go Back

Information

 
TitleOrder Tracking: Fixed Sampling versus Synchronous Sampling
URL Nameorder-tracking-fixed-sampling-versus-synchronous-sampling
Summary
Details


Direct YouTube link: https://youtu.be/q_Typy1TjMU


Fixed sampling and synchronous sampling are two different digital signal processing methods that can be used to calculate spectral maps and orders during a rotating machinery measurement.

Fixed sampling acquires data at a fixed data rate, while synchronous sampling acquires data at a rate proportional to the speed of the rotating machinery.

The results of each technique are shown in the colormaps in Figure 1 below. Fixed sampling gives a global overview of the speed sweep dynamics, while synchronous sampling has narrower and well defined orders.

Fixed_vs_Sync_Summary.png
Figure 1: Fixed sampling colormap (top) shows global view of speed sweep, including resonance. Order tracking colormap (bottom) based on synchronous sampling has narrower, better defined orders, but in this example, some resonance information is truncated.

Both techniques result in a colormap with three difference axes: frequency, rpm, and amplitude. However, the calculations involved in each technique are performed differently.

This article has the following sections:

1. How do fixed and synchronous sampling techniques work?
   1.1 Time versus Revolution Data Blocks
   1.2 Frequency Spectrum versus Order Spectrum
   1.3 Smearing in Fixed and Synchronous Sampling
   1.4 Preventing Smearing
2. Practical Differences in Results from Fixed Sampling and Synchronous Sampling
   2.1 Fixed Sampling Global View
   2.2 Synchronous Sampling: Narrow Orders
   2.3 Synchronous Sampling: Fast Speed Sweeps
3. Simcenter Testlab Classic: Settings and Displays
   3.1 Getting Started
   3.2 Fixed Sampling versus Order Tracking Settings

   3.3 Displays: Switching Axes between Order and Frequency


Note: Sometimes synchronous sampling is also called order tracking. The Simcenter Testlab software module that performs synchronous sampling is called ‘Order Tracking’.

1. How do fixed and synchronous sampling techniques work?

Both fixed sampling and synchronous sampling techniques calculate a series of spectrums at a defined tracking increment over a speed sweep.

1.1 Time versus Revolution Data Blocks

The difference in the two techniques is how the spectrums at each increment are calculated.

  • Fixed sampling is time based: At each increment, a Fourier Transform is performed on a fixed amount of time data (T). The Fourier Transform of a time block is a frequency spectrum, which consists of amplitude versus frequency. The same amount of time data is used for each Fourier transform regardless of system speed.
  • Synchronous sampling is revolution based: At each increment, a Fourier Transform is performed on a fixed number of revolutions (R), regardless of speed. The result is an order spectrum, which consists of amplitude versus order. As system speed changes, so too does the amount of time data used to calculate the order spectrum. As the rotational speed increases, the amount of time data required decreases as shown in Figure 2. The method is synchronized with the revolutions of the rotating system.

See Figure 2 for a comparison of the time data used for spectral calculations at four different speeds of the rotating system.

Time_versus_Revolutions.pngFigure 2: In fixed sampling (left), the time data block (T) used for the Fourier Transform remains the same throughout the speed sweep. In synchronous sampling (right), the time block varies, keeping the number of revolutions (R) the same, throughout the speed sweep.

Once the block of data is captured, either an order or frequency spectrum is calculated.

key1_time_rev.png

1.2 Frequency Spectrum versus Order Spectrum

Figure 3 shows the difference between the results of a Fourier transform for fixed sampled data versus the synchronously sampled data. The fixed sampling data produces a frequency spectrum, while synchronous sampling produces an order spectrum.

frequency_spec_versus_order_spec.png

Figure 3: Fixed sampling uses a time block (top left) that produces a frequency spectrum (top right) while synchronous sampling uses a revolution basis (bottom left) that produces an order spectrum (bottom right).

A key difference between the order spectrum and frequency spectrum is how data is spaced along the x-axis (see Figure 5):

  • Frequency spectrum – Spectral lines are a fixed frequency distance apart (delta f = 1/T)
  • Order spectrum – Spectral lines are a fixed order distance apart (delta o = 1/R) where R is the number of revolutions that the spectrum will be calculated over

A result of this is that order content can appear “smeared” when fixed sampled, but not when order tracked.

key2_spec_ord.png

1.3 Smearing in Fixed and Synchronous Sampling

In fixed sampling, the Fourier Transform requires a fixed time frame of data. During the fixed time frame, the speed of the rotating system changes. As the speed changes, the frequency of the order content also changes.

As the order content changes within the data frame, there is a leakage, sometimes referred to as smearing, of the order content as shown in Figure 4.

User-added image
Figure 4: Left – Frequency spectrum has a fixed frequency resolution (black dots on X-axis), which creates smearing (dashed green line) when frequency content changes with the increase in rpm. In the illustration, the rpm changes from 1000 to 1060 rpm. This causes a single peak of the measured system to change in frequency (from red peak thru gray peaks to blue peak) during the time required to perform the digital Fourier Transform.  Instead of a single peak (red or blue), a smeared peak appears (green).

If the rpm changes from 1000 rpm to 1060 rpm during the time required to perform a Fourier Transform, the frequency of 1st order would change by 1 Hertz (60 delta rpm change, divide rpm by 60 to get change in seconds rather than minutes, yields a 1 Hz change). This would create a smear 1 Hz wide because the peak changes frequency.

For other orders, the change would be even greater. For example, 4th order would create a 4 Hz smear during the same time period. This smearing effect is worse at higher orders (example: 54th, 72nd order) than lower orders (1st, 2nd, 3rd).

An order spectrum calculated from synchronous sampling does not have this smearing.  This is illustrated in Figure 5 below:

User-added image
Figure 5: Left - From a frequency perspective, as the rpm of the rotating system increases, the amount of time it takes to gather the fixed number of samples (per revolution) gets shorter, so the frequency resolution gets larger.  Right - The number of samples per revolution is constant, regardless of rpm, so the delta between order lines also remains constant.  With respect to time, the frequency of sampling increases along with increasing rpm.


The constant order resolution keeps spectral lines aligned with order frequencies, which prevents them from being smeared:

  • The sampling rate is adjusted constantly with respect to the rotational speed of the test object, even during the time needed to gather the data needed to perform a Fourier Transform.
  • The result is a spectrum with a fixed delta order width, rather than a fixed frequency width, between spectral lines.

key3_smeearing.png

1.4 Preventing Smearing

To reduce the smearing induced from the fixed sampling approach with respect to a changing rpm, three actions can be taken:

  1. Decrease speed sweep rate: If the speed sweep is slowed down, then the frequency content does not change as rapidly during the time block. For example, instead of taking 10 seconds to sweep from 1000 rpm to 6000 rpm, a longer time of 100 seconds could be used.
  2. Change spectral resolution: The time frame analyzed (and thus the change in rpm) can be shortened by making the spectral resolution more coarse. This reduces smearing induced by the change in rpm.  (The spectral resolution inversely related to the time frame: A 0.5 Hz resolution corresponds to a 2 second frame, a 0.25 Hz resolution corresponds to 4 seconds). This is a trade-off and may require adjustment.  A coarser frequency resolution potentially creates leakage that could offset the reduction in leakage due to the smaller change in rpm.
  3. Use a synchronous sampling technique instead of fixed sampling.

There are several key settings that can affect the processed results.

Processing Parameters

Table 1 below lists the equations and parameters used in the two techniques.

User-added image
Table 1: Parameters and settings used in fixed sampling and synchronous sampling.

These same settings are illustrated in the diagrams in Figure 6.

deltaf_vs_deltao.png
Figure 6: Left –In fixed sampling, the spectral lines are fixed delta frequency apart, which are not aligned with the order content. In synchronous sampling, the spectral/order lines are a fixed delta order apart, which stays aligned with the order content even as rpm changes.

The next section illustrates the differences in the calculated results between fixed sampling and synchronous sampling results.

2. Practical Differences in Results from Fixed Sampling and Synchronous Sampling

This section shows how the results differ between fixed sampling and synchronous sampling. See Table 2 below for a summary of the key differences between each of the techniques:

table2.png
Table 2: Summary of differences between fixed sampling versus synchronous sampling results.

These difference are illustrated in the next sections.

2.1 Fixed Sampling: The "Global" View

A key benefit of fixed sampling is the “global view” that it provides as shown in Figure 7.

fixed_sampling_global.png
Figure 7: Fixed sampling provides a good global view of the system by demonstrating clear lines of resonance alongside order content.

Fixed sampling highlights both resonance information alongside with the order information. In a fixed sampled map, resonances appear as vertical lines at fixed frequencies.

key4_global.png

2.2 Synchronous Sampling: Narrow Orders

The benefit of using synchronous sampling is that a much finer order resolution can be achieved.

Look at Figure 8 below for an example of this. The orders are narrower and better defined on the synchronous sampling colormap plot (right) compared to the fixed sampling plot (left).

smeared_orders.png

Figure 8: Left – Fixed sampled colormap (left graph) has wider orders (red) than the synchronously sampled colormap (right graph).

Because orders tend to be smeared more on fixed sampled data, caution must be used when performing order cuts. The width of the order cut is very important: when cutting an order from fixed sampled data, care must be taken to ensure that the width of the order is selected to properly contain the order content.

Example:

Order 10.5 is cut from both the fixed sampled and synchronous sampled plots from above (see Figure 9, below).

vary_order_width.png
Figure 9: Order cut comparison: Using the same order cut width of 0.2, the orders do not match (left graph). A wider order cut must be used on the fixed sampled data to ensure the proper match (right graph).

The same order width (0.2) is used for both cuts (Figure 8, left graph). Notice that the fixed sampled order (red) appears to be lower level than the order tracked order (green). This is because the order content for the fixed sample order has smeared beyond the 0.2 order width bandwidth. Therefore, the order cut is not capturing all of the energy content of the order.

However, if the order width of the fixed sampled data is increased to 0.4 order width, the results between fixed and synchronous sampling compare much more closely (Figure 8, right graph).

This is especially important when a rotating system has closely spaced orders. If significant smearing is present in a fixed sampling technique, it can be impossible to separate the orders and get the correct results, because the adjacent orders smear together.

key5_close_orders.png

For example, if a piece of rotating machinery made two orders: 10.1 and 10.3, a smearing of 0.4 order would not produce correct results for these orders.

2.3 Synchronous Sampling: Fast Speed Sweeps

Another area in which synchronous sampling has an advantage is fast speed sweeps. The faster the rpm changes, the more the frequency content changes over time.

The synchronous sampling techniques reduces the smearing of the orders that are caused by a fast speed sweep as shown in Figure 10.

slow_versus_fast_runups.png
Figure 10: Upper Left – Fast sweep and fixed sampling have order smearing, Upper Right – Fast sweep with sync sampling does not have order smearing, Lower Left – Slow sweep with fixed sampling has no smearing, Lower Right – Slow sweep with sync sampling has no smearing.

In Figure 10, the difference between fixed sampling and synchronous sampling on a 4 second “fast” sweep and a 20 second “slow” runup is shown. For the same data orders, the fixed sampling data for the four second runup shows order smearing. The higher number orders also have more smear.

key6_runup_speeds.png

Either by slowing down the speed sweep, or by switching from fixed sampling to synchronous sampling, the order smearing can be reduced.

The next section explains how to perform fixed and synchronous sampling on speed sweep data in Simcenter Testlab.

3. Simcenter Testlab Classic: Settings and Displays

Both fixed sampling and synchronous sampling can be done in Simcenter Testlab Classic. Both methods can be used simultaneously while processing the same data.

When using Signature Acquisition or Signature Throughput processing, the fixed sampling approach is used by default. However, synchronous sampling can also be turned on via the ‘Order Tracking’ add-in and used in parallel with the default fixed sampling.

3.1 Getting Started

Enable synchronous sampling by selecting “Tools -> Add-ins -> Order Tracking” from the main Simcenter Testlab menu as shown in Figure 11.

order_track_addin.png
Figure 11: To perform synchronous sampling in parallel with fixed sampling, select “Order Tracking” under “Tools -> Add-ins”.

The Order Tracking add-in requires 20 tokens.

3.2 Fixed Sampling versus Order Tracking Settings

In Figure 12, the Fixed Sampling and Order Tracking settings in Signature Throughput Processing are shown. The Fixed Sampling settings are under the tab called “FS Acquisition” while the Order Tracking settings are under the tab called “OT Acquisition”.

fixed_vs_order_settings.png
Figure 12: Left – Fixed Sampling settings for 0.125 second frame size, Right – Order Tracking settings for 0.125 order resolution.

There is a fixed relationship between frequency, rpm, and maximum order, as shown in Equation 1:

equation.png
Equation 1: Relationship between frequency, rpm, and order.

When the maximum frequency of the acquisition, or bandwidth, is used in Equation 1, the maximum order and corresponding rpm can also be determined. These settings and relationships are also described in Table 1 above.

For example, the software menus shown in Figure 11 indicate that 16th order can be measured up to 24000 rpm with a given frequency bandwidth of 6400 Hz. This uses the equation: [6400 Hz = (16 * rpm)/60]. This maximum rpm is automatically calculated (Figure 11, right graph). To go to a higher rpm, and still measure 16th order, the frequency bandwidth would need to be increased.

Engineers will often calculate both fixed sampled and order tracked results to get the benefits of both types of data processing.

3.3 Displays: Switching Axes between Order and Frequency

In Simcenter Testlab, it is possible to switch between frequency and order on the plot axis.

For a fixed sampled map, simply right click on the X Axis, and select “X axis -> Frequency or Derived Order” as shown in Figure 13.

switch_axes_1.png
Figure 13: On a frequency spectrum map, right click on the X axis to switch between frequency and derived order.

For an order tracked map, simply right click on the X-axis and make the selection for either “Order” or “Derived Frequency” as shown in Figure 14.

switch_axes_2.png
Figure 14: On an order spectrum map, right click on the X axis and choose between order and derived frequency.

Questions? Email scott.beebe@siemens.com or Siemens Support Center.

 

More Rotating Machinery Links:

More Digital Signal Processing Links:


Powered by