Salesforce

Simcenter Testlab Throughput Processing Tips

« Go Back

Information

 
TitleSimcenter Testlab Throughput Processing Tips
URL Namesimcenter-testlab-throughput-processing-tips
Summary
Details


Direct YouTube link: https://youtu.be/jtDi09haYGE

 

Simcenter Testlab Throughput Processing Tipslogo.png

Data processing can be an arduous task, but it does not have to be! Here are some tips for navigating the processing settings and organizing results.

Getting Started

In Simcenter Testlab (formerly called LMS Test.Lab), any time data can be analyzed using the Time Data Processing worksheet (Picture 1) which is located at the bottom of the screen.

TimeDataProcessingWorksheet.png
Picture 1: Processing of throughput files can be done in the Time Data Processing worksheet.

This worksheet can be accessed via Tools -> Add-ins -> Signature Throughput Processing (Picture 2). Signature Throughput Processing requires 36 tokens.

ThroughputProcessingAddIn.png
Picture 2: Turn on throughput processing by selecting “Tools -> Add-in” in the main menu.

After pressing “OK” in the Add-in menu, the Time Data Processing worksheet should appear as a new worksheet at the bottom of the screen. Any data selected in the Time Data Selection worksheet can be processed.

See the article below are three tips for using throughput processing:

  1. Measurement Mode: Stationary versus Tracked
  2. Data Naming
  3. Original Section versus Active Section

1. Measurement mode: Stationary versus Tracked

In the Time Data Processing worksheet, a major data processing choice is made by selecting either ‘Tracked’ or ‘Stationary’ measurement mode under “Change Settings” in the “Acquisition Parameters” section.

traced_vs_stationary.png
Picture 3: The Acquisition parameters menu contains Tracked versus Stationary choices for measurement mode.

One can select between ‘Tracked’ and ‘Stationary’ measurement mode (Picture 3). Depending on which one is selected, the processed data results will be very different.

Stationary measurements

When ‘Stationary’ Measurement mode is selected, the processed results consist of a single averaged spectrum for each time data channel (Picture 4).

stationary.png
Picture 4: Stationary mode results in single averaged spectrum

When should stationary mode be used?

Imagine that the issue you are tasked with occurs only when the engine is at 2400 rpm. You can measure using the stationary method at 2400 rpm for 30 seconds. The results will show you a single spectrum revealing the highest amplitude frequencies so you can apply damping or other countermeasures to solve the issue.

In stationary mode, one can specify free run averaging with a specific overlap. Different types of averaging methods (maximum, minimum, average, etc) can also be selected.

Tracked measurements

Setting ‘Tracked’ for the measurement mode results in several spectra at user defined increments. With this mode it is easy to visualize how the data changes as a function of time, rpm, or angle (Picture 5).

Imagine you work for an automotive manufacturer and customers are complaining about a noise they hear while driving. You are tasked with solving the issue but the only information you are given is that the noise gets worse as engine rpm increases. You can instrument the vehicle with accelerometers, microphones, and an engine tachometer on the drive shaft. Using the tracked method, you can identify any high amplitude signals that change with engine rpm. In throughput processing, one can perform order analysis.

tracked.png
Picture 5: Tracked mode results in a series of spectrums which can be displayed in a waterfall graph

Tracked processing: Increment and Frame Settings

Often when using tracked processing, a tachometer is specified as a tracking channel (Picture 6). For example, one might process data from 1000 to 3000 rpm in increments of 25 rpm using the tachometer tracking channel.

frame_vs_increment.png
Picture 6: Frame size and increment settings used in tracked throughput processing

Tracked processing results in a buildup of several frequency functions, usually calculated spectra, and are often displayed in three dimensional plots called waterfalls (Picture 7) or colormaps. Each curve in the waterfall display is a separate processing calculation (or measurement), taken from the raw time data. It is calculated based on user defined acquisition parameters, namely the increment and frame size.

Increments are the intervals between frame calculations. These intervals are usually either time or rpm based. For example in the Picture 7, a spectrum is calculated every 25 rpm, therefore our increment is 25 rpm.

waterfall.png
Picture 7: Waterfall graph showing tracked spectrums based on rpm

If tracking on time, the increment is the time interval (in seconds) between acquisitions.

Picture 8 illustrates points of data acquisition in time at 1 second, 2 second, and 0.25 second increments.

increment.png
Picture 8: Various processing increments – Top: 1 second, Middle: 2 seconds, Bottom: 0.25 seconds

The frame size is the how much data is used for a calculation at each interval. For example, an increment of 0.5 seconds and a frame of 1 second, would result in overlap processing of 50%.

When windows, such as Hanning windows, are used they are applied to the frame.

frame.png

Picture 9: Illustration of different frame sizes for data processing – Top: 1 second frame, Middle: 2 second frame, Bottom: 0.25 second frame

The relationship between the size of the increment and the size of the frame determines what data is used for processing. Depending on the setting, it is possible that some data will not be used (ie, data “gaps”) or that some data will be used multiple times (ie, data “overlap”).

frame_vs_inc_illustration.png
Picture 10: Increment versus Frame size illustrations

One frame of data is collected, modified with a window, and reported as a single data point. The increment is the time between these data points.

When the frame size and increment match, all data are processed with no overlap, meaning no missed data (Picture 11). However, if there was a window applied, an amplitude and/or energy error could occur. This is because a Hanning window zeros much of the data at the beginning and end of the frame. If a large event coincided with the beginning of a frame, the Hanning window would significantly reduce the amplitude.

zero_overlap.png
Picture 11: 0% Overlap for processing of data when frame size and increment are equal

 

Using a frame size larger than the increment can help with that (Picture 12). The ‘overlap’ allows more averages within the time duration of the test and helps reduce the error associated with the window.

overlap.png

Picture 12: 10% Overlap for processing data, increment is smaller than frame size


The combination of the frame size and increment determines the overlap. For example, frame size of 1 second, with a 0.5 second increment, corresponds to a 50% overlap.

For more insight into how overlap is affected by the sweep rate, see the Knowledge Base article: Speed Sweep Data Processing: RPM Increment, Framesize, Sweep Rate, and Overlap.

2. Data Naming

By default the results from a Throughput Processing calculation are saved into the active section under a new run name. The default is “Tp” which is an abbreviation of “Throughput Processing”.

When looking back at processed data, if they are all named “Tp 1”, “Tp 2”, “Tp 3”, rather than “Run 1 with High Load”, “Run 2 with Medium Load”, “Run 3 with Low Load”, it can be difficult to tell which run the data came from originally, which is useful information when analyzing and reporting.

RunName.png
Picture 13: In the center of the Time Data Processing worksheet, click on the button labelled “…” allows different run naming options

The button next to the Name field opens the ‘Results destination options’ window (Picture 13). If the ‘Run name’ setting is changed to ‘Run Name Postscript’ the results will be saved into a new run as before, but with the new run name appended to the original run name making it easy to tell where the data came from as shown in Picture 14.

RunName2.png
Picture 14: The ‘Run Name Postscript’ option contains the original run name and appends the extension. The ‘Run name’ option does not preserve the original name.

If data was processing without the ‘Run Name Postscript’ enabled, one can still find the original run name in the data properties.

DataProperties.png
Picture 15: Original run data properties

Right click on any processed data and select “Properties” to see information like:

  • Original project
  • Original project dir
  • Original run
  • Orignal section

3. Original Section versus Active Section

Take a Simcenter Testlab project (*.lms file extension) with two sections: ‘Baseline’ and ‘Modified’. Three data acquisition runs were performed in a baseline condition, and three runs were done in a modified condition.

TwoSectionsThreeRuns.png
Picture 16: LMS Test.Lab project with two sections and three runs with the same names

Both the ‘Baseline’ and ‘Modified’ section contain runs with the same name: “Run 1”, “Run 2”, and “Run 3” as shown in Picture 16.

If all six runs are processed at once, the default “Active section” setting in Throughput processing would create multiple runs of similar names in one section (Picture 17). This is confusing, because it is not clear which runs are associated with ‘Modified’ and which as associated with ‘Baseline’.

ActiveSection.png
Picture 17: Throughput processing of all 6 runs with “Active Section” set and “Run name postscript”. Data is mixed.

When performing throughput processing, there is an important setting that can avoid this confusing situation (Picture 18). The ‘Save Destination’ can be changed from the default ‘Active Section’ to ‘Original Section’.

OriginalSectionMenu.png
Picture 18: The ‘Save Destination’ can be switched between ‘Active Section’ and ‘Original Section’

After processing the data, it is clear which data is from the ‘Baseline’ section and which data is from the ‘Modified’ section as shown in Picture 19.

OriginalSection.png
Picture 19: With ‘Original Section’ all processed data returns is clearly stored with original source

Note that if “Original Section” is selected, one must have the original project open.

Time files that are located outside the currently opened project cannot be processed with the ‘Original Section’ setting. This is because processed data can only be stored in the currently open project.

Conclusion

Want to process data with certain orders removed?  Check out the Knowledge article "Simcenter Testlab: Recalculating Levels with Orders Removed".

Hope you find these tips helpful for using Throughput Processing! 

 

Questions? Email scott.beebe@siemens.com or contact Siemens Support Center.

 

Related Simcenter Testlab Processing Tips:

Simcenter Testlab Acquisition Tips:

Simcenter Testlab Display Tips:


Powered by