Salesforce

Octaves in Human Hearing

« Go Back

Information

 
TitleOctaves in Human Hearing
URL Nameoctaves-in-human-hearing
Summary
Details


Direct YouTube link: https://youtu.be/JMGFAz3TEUc


Octaves are groups of frequencies that help quantify how humans distinguish between frequencies as shown in Figure 1.

1.png

Figure 1: An octave map. Each vertical block is an octave and represents the overall level of sound energy over that range of frequencies.


Octaves represent the overall level of energy over a specific frequency range.

This octave article has the following sections:
1. How are Octave Bands Determined?
2. Octave Spacing
3. Octave Standards
4. How Octaves Are Calculated
5. Calculating Octaves in Simcenter Testlab
6. Octave Displays in Simcenter Testlab
   6.1 Octave Display
   6.2 FrontBack Display

 

1. How are Octave Bands Determined?

The term “octave band” is borrowed from music theory (Figure 2) where there is a doubling of frequency between notes of the same name.
 

2.png
Figure 2: In music, there is a doubling of frequency between notes of the same name.


Octave bands in human hearing are developed in the same manner: the range of human hearing (20-20kHz) is divided into eleven octave bands, each band having double the frequency span of the previous band. These are called the 1/1 octave bands as shown in Figure 3.
 

3.png
Figure 3: The lower, upper, and center frequencies of the 1/1 octave bands over the human hearing range.

 

To more closely match how humans distinguish frequencies, each 1/1 octave band can be split into three bands. These are called the 1/ 3 octave bands and listed in Figure 4 below.
 

4.png
Figure 4: The upper, lower, and center frequencies for the 1/3 octave bands.

These smaller bands more closely represent how humans distinguish between frequencies.


2. Octave Spacing

Octaves are often displayed so that the center frequencies of the octave bands are linearly spaced. This is called octave format. This causes the octaves to appear equally spaced in frequency even though they are not.

In Figure 5 below, white noise is expressed in both narrow band (blue) and octave format (green). The x-axis is in octave format (described above). Notice that the octave bands at lower frequencies have less data filling them compared to the octaves at higher frequencies (Figure 5). This is because octave bands at higher frequencies cover a broader frequency range than octave bands at lower frequencies.
 

5.png
Figure 5: X-axis in octave format. The same random white noise is expressed in octaves and as an autopower.

 

The same data is plotted below but the x-axis is in linear format. Notice that an autopower (blue) has the same density at all frequencies. Notice that the range of frequencies each octave band (green) covers gets larger and larger as shown in Figure 6.
 

6.png

Figure 6: X-axis in linear format. The same random white noise is expressed in octaves and as an autopower.


Octave bands help determine how the human ear distinguishes between frequencies. At lower frequencies, the ear can more easily distinguish between frequencies. Thus, the octave bands are narrower. At higher frequencies, the ear has difficulty distinguishing between frequencies (even frequencies that are somewhat far apart). Thus, the octave bands are wider. Watch the video below to hear this phenomenon.

 


Direct YouTube link: https://youtu.be/9GxF-OVYwW8
 

NOTE: Critical bands are also used for defining frequency determination by the human ear. The critical band scale is slightly more refined compared to octaves. Critical bands (like octaves) are used in the determination of many sound quality metrics.

3. Octave Standards

Some standards that define how octaves are calculated:

  • American National Standards Institute (ANSI) S.1.11: Specification for Octave, Half-Octave, and Third Octave Band Filter Sets
  • International Electrotechnical Commission (IEC) 61260: Specifications for Octave-band and Fractional-Octave-band Filters


4. How Octaves Are Calculated

Octaves are calculated using a series of time-domain based, band-pass filters.

Time data is fed into a series of narrow-band filters as shown in Figure 7. Each filter band represents the frequency range of each octave. In Simcenter Testlab, the filter shapes conform to the ANSI and IEC standards.
 

7.png

Figure 7: Time data is fed through narrow band filters. Each filter represents an octave band. The overall level of the time data is plotted on a per-octave basis and then plotted.

Both octave maps (like in the figure above) and octave sections can be calculated.

  • Octave maps plot the octave bands vs. the overall level of energy in those bands.
  • Octave sections track how a single octave band behaves against a tracking parameter.

For example, Figure 8 below shows how the 12.5 Hz, 20.0 Hz, and 25.0 Hz octave bands change with time.

8.png

Figure 8: An octave section tracks how an octave behaves against a tracking parameter. In this case, it is tracking the octave against time.

Depending on the application, an average level of the octave may also be calculated, rather than displaying it against time.


5. Calculating Octaves in Simcenter Testlab

To calculate filter based octaves in Simcenter Testlab (formerly called LMS Test.Lab), go to “Tools -> Add-ins” and turn on “ANSI-IEC Octave Filtering” (Figure 9). This add-in requires 23 tokens.
 

9.png

Figure 9: Turn on “ANSI-IEC Octave Filtering”.
 

In Time Data Processing, open the “Acquisition parameters” settings button (“Change Settings”) as shown in Figure 10.
 

10.png

Figure 10: The change settings dialog for octave averaging.

Select an averaging method: exponential or linear. The exponential average weights the acquisitions taken later in time more heavily than earlier acquisitions. The linear average calculates the arithmetic mean of all the values.

Select a sound level type: fast (0.125 sec), slow (1.000 sec), impulse (0.035 sec), or user (custom). This parameter changes the length of the averaging frame. The averaging frame is the length of time that is used to calculate an average at every increment. Check out the Simcenter Testlab Throughput Processing Tips article for more information about increment and frames.

In Time Data Processing, open the “Section” settings button by clicking “Change Settings” under “Section. To calculate an octave map, go to the “Octave Maps” tab. Check on the octave band type that needs to be calculated as shown in Figure 11.
 

11.png

Figure 11: Calculating octave maps. In this case, 1/3 octaves will be calculated.

A result of this calculation would look something similar to Figure 12 below.
 

12.png

Figure 12: The result of an “octave map” calculation.


To calculate a single octave section, go to the “Octave Sections” tab. Type in the center frequency of the octave section(s) that is desired to be calculated as shown in Figure 13.
 

13.png

Figure 13: Octave sections to be calculated.

The octave section calculation will calculate how an octave behaves vs. a tracking parameter. Figure 14 below gives an example of the result from this calculation.
 

14.png

Figure 14: Example of how various octaves behave vs. time.

NOTE: There are a few additional tabs with the RTO (Real Time Octaves) suffix. Anything with the suffix RTO will used filter-based octaves to do processing. For example, “Psychoacoustic Metrics RTO” uses time-based filters to calculate sound metrics.


6. Octave Displays in Simcenter Testlab


Direct YouTube link: https://youtu.be/2FB1QOoPdeM


Octave data can be displayed using two different methods in Simcenter Testlab: the Octave Display and the FrontBack display:

6.1 Octave Display

There is a special display in Testlab called the “Octave Display".  Data dropped into the display will always be shown in octaves. 

The icon use to open the display is enlarged and shown in Figure 15 below.
 

15.png

Figure 15: The octave display icon opens an octave display.

The octave display automatically puts the x-axis in octave format. It also automatically puts data into a “block display” format (as octaves are traditionally displayed in).

When data is dropped into an octave display, it will look similar to Figure 16 below:

12.png

Figure: 16: Octave Display

Even a narrowband spectrum will be converted to octave format when dropped in the display.

6.2 FrontBack Display

If data is already in octave format, the FrontBack display can be used to display it as shown in Figure 17:

User-added image

Figure 17: The FrontBack display can be used to display octaves and the corresponding narrowband spectrum overlaid.


To display octave data in the FrontBack display, here are some common settings:

  • Y-Axis in dB: Right click on Y-axis and change format to dB.
  • X-Axis in Octave: Right click on X-axis and change format to octave.
  • Curve Style: Right click on data and choose "Curve Style...".  Set Trace Style to "Blocks" or "Block Outlines".  Change the "Outline color" if desired.

With the FrontBack display, both narrowband and octave data can be overlaid.  This can yield useful insights. For example, the exact frequency of a tone that is causing an octave band to be higher than the rest can be identified.


Questions? Email Scott MacDonald (macdonald@siemens.com), contact Siemens Support Center, or reply to this article.

 

Related Links:


Powered by