Salesforce

Q: How can I overlay multiple signals in one y axis over one signal on the x axis in Simcenter Tecware?

« Go Back

Information

 
TitleQ: How can I overlay multiple signals in one y axis over one signal on the x axis in Simcenter Tecware?
URL Nameq-how-can-i-overlay-multiple-signals-in-one-y-axis-over-one-signal-on-the-x-axis-in-lms-tecware
Summary
Details

Q: How can I overlay multiple signals in one y axis over one signal on the x axis in Simcenter Tecware?

A: You can either use the default Reporting job xy.tbd. But this uses pairs of x,y,x,y,x,y,... channels to build the x/y diagrams. Having one signal on x and multiple y axis would mean to duplicate the x signal many times.

To avoid this, you can also use Simcenter Tecware ProcessBuilder. The attached job (copy *.pb and *.aly into the same directory and load the *.pb in ProcessBuilder).

2016-04-17 20_43_59-LMS Tecware ProcessBuilder_ D__Topics_GM_xy_Report xyyy.pb.png

Now, change the selection in Pass_DataX to select your X signal and make sure all Y signals are selected in Pass_Data2. That's it. Run the process and check out the report in Microsoft Word:
2016-04-17 20_54_14-Tempxyreport_2.doc [Compatibility Mode] - Word.png

Load multiple files with the same x,y channel setup and you will get one diagram per file on different pages.

In order to use the attached process, you should have at least  Simcenter/LMS Tecware 3.11 installed.

More Fatigue and Durability links:

Simcenter Tecware Links:


Powered by