Salesforce

What's New in Simcenter Testlab 2606

« Go Back

Information

 
TitleWhat's New in Simcenter Testlab 2606
URL NameWhat-s-New-in-Simcenter-Testlab-2606
Summary
Details
Simcenter Testlab 2606 is here! 
  • Simcenter Testlab 2606 was released in June 2026. "2606" is 26 for the year 2026 and 06 for the month of June.
  • Previous release was Simcenter Testlab 2506.
Check out the new features of Simcenter Testlab 2606 below:
 
OVERVIEW 

 
Direct YouTube link: https://youtu.be/lKunIqv7a2g

 
  • New distinct icons for Simcenter Testlab Neo (TLN) and Simcenter Testlab Classic (TLC).
User-added image
  • Software revision (2606) is part of application name.
  • Help file default installation points to website, saves over 2 Gb of space.
  • Updated color scheme (black and green), no longer contains blue color.
User-added image
The new color scheme of Simcenter Testlab is black and green, no longer features blue color.
 
ACOUSTICS 
  • Audio replay allows switching between different sounds based on rpm in addition to time.
  • 3 microphone transmission loss added in addition to 4 microphone transmission loss.
User-added image
Three microphone transmission loss method for impedance tubes in Simcenter Testlab Classic.
 
DISPLAYS 
User-added image
The "Automatic Queries" options will create a query for data in the displays whenever possible.
 
ENVIRONMENTAL 


Direct YouTube link: https://youtu.be/R1hOsP5Mk4Y 

New features of Simcenter Testlab Dynamic Environmental (closed loop vibration control products like sine, random, shock, etc):
  • Compare Models: Easy comparison and overlay of System Identification (SI) results for comparing test setups.  Also for comparing virtual shaker setups to physical tests.
  • Acoustic control enhancements: Completing the acoustic control suite from Reverberant Chambers to Progressive Wavetubes to Direct Field.
  • Half periods wavelets in Shock Control Synthesis (SRS): Used to ensure displacement begins and ends at zero for shock pulses
  • Improved logging of notching/limiting in Random Control: Not just the largest notch is logged, all notches are logged.
  • Neo Mission Synthesis: Three additions include PSD Confidence interval, easier definition of repetitive events, saving of individual mission FDS and SRS results in addition to total.
 
GENERAL ACQUISITION 


Direct YouTube link: https://youtu.be/TcXYhbG7ctc 
 
 
MODAL TESTING 


Direct YouTube link: https://youtu.be/F1Jxvd428iI 
 
 
MODAL ANALYSIS 


Direct YouTube link: https://youtu.be/-N8fMFBtgkw
 
PROCESSING 


Direct YouTube link: https://youtu.be/v3dn0mcoFS8
 
  • Block Editor available in Simcenter Testlab Neo to be able to create limit lines, import data from Excel, edit block data.
  • Process Designer:
    • Option Save to Original Run
    • New "Print to Preview" method
    • Block Calculator method: Integration/Differentation
    • Block Calculator method: X-axis
    • Map Calculator method now works with orders, tonality, roughness, modulation maps.
    • Multiplex/demultiplex methods to create stereo channels
    • Block Smoothing method
    • Print to PowerPoint automatically when running process
  • Offline RPM Extraction available as interactive workbook in addition to previous method in process designer
User-added image
Interactive Offline RPM extraction workbook in Simcenter Testlab Neo
 
TRANSFER PATH ANALYSIS 


Direct YouTube link: https://youtu.be/aMeyH679-G8
 
  • Mount force estimation method added in addition to existing direct and matrix inversion force methods.
  • Adaptative Tikhonov option added to Singular Value Decomposition method
  • FRF Based Decoupling to remove test rig and other dynamic influences
More information: Simcenter Testlab Neo NVH Prediction 2606
 
INSTALLATION 

Simcenter Testlab 2606 available: Simcenter Testlab 2606: Download and Install Instructions

Past releases:

Powered by